LVDS clock on i.MX6 in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS clock on i.MX6 in u-boot

1,780 Views
andreas81
Contributor I

Hi,

we are working with self-developed i.MX6 board. Now we have enabled U-Boot splash screen support. It is working well, but we have problems with LVDS interface.

If we configure LVDS we always get 56MHz LVDS clock although we configured 30MHz for LVDS clock via displays structure in the board file:

      .bus  = 0,

      .addr = 0,

      .pixfmt     = IPU_PIX_FMT_RGB24,

      .detect     = NULL,

      .enable     = enable_lvds,

      .mode = {

            .name           = "wvga-lvds",

                .refresh        = 57,

                .xres           = 800,

                .yres           = 480,

                .pixclock       = 33000,

                .left_margin    = 40,

                .right_margin   = 40,

                .upper_margin   = 3,

                .lower_margin   = 80,

                .hsync_len      = 10,

                .vsync_len      = 10,

                .sync           = FB_SYNC_EXT,

                .vmode          = FB_VMODE_NONINTERLACED

Has anyone an idea what's going wrong?

Best regards,

Andreas

Labels (1)
0 Kudos
Reply
3 Replies

1,097 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Andreas,

    try to modify clock source of LVDS to be PLL5 (pll5_video_mail_clk), please!  The current source should be from IPU (264MHz).

Regards,

Weidong

0 Kudos
Reply

1,097 Views
andreas81
Contributor I

Hi Weidong,

Thanks for your help.

Can you advise me which is the correct register to set PLL5 as clock source?

Best regards,

Andreas

0 Kudos
Reply

1,097 Views
laszlotimko
Contributor III

Hi,

Here is an example:

--- arch/arm/mach-imx/clk-imx6q.c.dist

+++ arch/arm/mach-imx/clk-imx6q.c

@@ -488,6 +488,10 @@

        clk_register_clkdev(clk[IMX6QDL_CLK_GPT_3M], "gpt_3m", "imx-gpt.0");

        clk_register_clkdev(clk[IMX6QDL_CLK_ENET_REF], "enet_ref", NULL);

+       /* Set LDB_DI_SEL parent to be PLL5 */

+       imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI0_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);

+       imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI1_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);

Regards

0 Kudos
Reply