LVDS clock on i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS clock on i.MX53

Jump to solution
1,244 Views
samarthmehta
Contributor II

Hi, all,

I need a frequency of 33.26 MHz for the LVDS clock signal, but I am getting 66 MHz.

I have added the following mode to the ldb_modedb[] array in /drivers/video/mxc/ldb.c and mx53_evk.c:

{

     "SVGA", 60, 800, 480, 30066,

     128,128,

     23, 22,

     0, 0,

     FB_SYNC_CLK_LAT_FALL,

     FB_VMODE_NONINTERLACED,

     0

,},

My LCD is working, but display is stretched out unless I use pixel clock as 17250 instead of 30066.  Regardless of what pixel clock value I use, I get 66 MHz on LVDS clock line, which is out of spec for LCD and it puts noise on our boards. 

I am using i.MX53 and freescale version of Linux kernel 2.6.35.

Can you please guide me where I need to change clock frequencies to achieve 33.26 MHz?

Thanks

Labels (3)
Tags (4)
0 Kudos
Reply
1 Solution
829 Views
samarthmehta
Contributor II

I changed

unsigned long ldb_clk_prate = 455000000;

to

unsigned long ldb_clk_prate = 229292424;

in ldb.c

This brought 66 MHz clock to 33.1 MHz.

View solution in original post

0 Kudos
Reply
3 Replies
829 Views
igorpadykov
NXP Employee
NXP Employee

Hi Samarth

had you passed correct kernel parameter, examples can be found in

MX53UG 18.3.1 Setting the Video Kernel Parameter and in Table 5-1

i.MX53_START_Linux_BSP_Release_Note.pdf in IMX53_1109_LINUXDOCS_BUNDLE    

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
829 Views
samarthmehta
Contributor II

Hi igor,

My kernel parameters are below:

bootargs_base=setenv bootargs console=ttymxc4,115200 video=mxcdi1fb:RGB666,SVGA di1_primary ldb=separate,di=0,di=1,ch0_map=SPWG,ch1_map=SPWG consoleblank=0

They seem right to the best of my knowledge.  I think the problem is the way PLL is getting set.  I am not sure where to change it.  It must be either in ldb.c or clock.c.   I will look deeper into it.  Someone has a same problem on i.MX6 and they changed the clk-imx6q.c.  We don't have this file on linux-2.6.35 and we use i.mx53, so it makes sense that it is absent.  See LVDS pixel clock on i.MX6 for more details.

0 Kudos
Reply
830 Views
samarthmehta
Contributor II

I changed

unsigned long ldb_clk_prate = 455000000;

to

unsigned long ldb_clk_prate = 229292424;

in ldb.c

This brought 66 MHz clock to 33.1 MHz.

0 Kudos
Reply