LVDS Display resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LVDS Display resolution

跳至解决方案
2,964 次查看
pankajrana
Contributor III

What is the maximum resolution we can get by using only one LVDS Channel.?? As per information I think it is not possible to achieve 1080p HD resolution by using only one LVDS channel.

There is a 31.5 inch LVDS Display, having two channel input, and resolution 1920x1080. How is it possible to increase the resolution to get Full HD 1920x1080 ? i.e. what input must be supplied to the LCD input pins,?

标签 (6)
0 项奖励
回复
1 解答
1,917 次查看
saurabh206
Senior Contributor III

Hi,

If you don't use split mode than you will not get the 1080P.

Dual Mode is used to display same data on two display.

You can try if you want, and share your result.

Thanks

Saurabh

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,917 次查看
pankajrana
Contributor III

SergioSolis SaurabhPatel

Hello All,

Split mode is understood, but what if I don't go for SPLIT mode, instead I choose Dual Channel Mode.
i.e. Using only channel one , and then providing the same data to both the input ports of the Display.?

will that give a proper image/display, or will it spoil the contents !

Thanks.

Pankaj Rana

0 项奖励
回复
1,918 次查看
saurabh206
Senior Contributor III

Hi,

If you don't use split mode than you will not get the 1080P.

Dual Mode is used to display same data on two display.

You can try if you want, and share your result.

Thanks

Saurabh

0 项奖励
回复
1,917 次查看
saurabh206
Senior Contributor III

Hi,

To get 1080P you need to use two channel.

Saurabh

0 项奖励
回复
1,917 次查看
pankajrana
Contributor III

Hi Saurabh,

Using two channels is fine, even the Display supports that, but am worried about the mode to be used, Should I go with Dual Channel Mode , or Split Channel mode ?

Thanks.

Pankaj Rana

0 项奖励
回复
1,917 次查看
saurabh206
Senior Contributor III

Hi

You should use Split channel mode to get 1080P working...

Saurabh

1,917 次查看
SergioSolis
NXP Employee
NXP Employee

Yes, you can achieve 1080p by using split channel mode.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------