Hello,
I am a little confused with the internal dsi to lvds bridge on the imx8mp device tree configuration. On the fsl,ldb.yaml example is like below:
#include <dt-bindings/clock/imx8mp-clock.h>
blk-ctrl {
#address-cells = <1>;
#size-cells = <1>;
bridge@5c {
compatible = "fsl,imx8mp-ldb";
clocks = <&clk IMX8MP_CLK_MEDIA_LDB>;
clock-names = "ldb";
reg = <0x5c 0x4>, <0x128 0x4>;
reg-names = "ldb", "lvds";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
ldb_from_lcdif2: endpoint {
remote-endpoint = <&lcdif2_to_ldb>;
};
};
port@1 {
reg = <1>;
ldb_lvds_ch0: endpoint {
remote-endpoint = <&ldb_to_lvdsx4panel>;
};
};
port@2 {
reg = <2>;
ldb_lvds_ch1: endpoint {
};
};
};
};
};
ldb node for the evk is like below:
ldb: ldb@32ec005c {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx8mp-ldb";
clocks = <&clk IMX8MP_CLK_MEDIA_LDB_ROOT>;
clock-names = "ldb";
assigned-clocks = <&clk IMX8MP_CLK_MEDIA_LDB>;
assigned-clock-parents = <&clk IMX8MP_VIDEO_PLL1_OUT>;
gpr = <&media_blk_ctrl>;
power-domains = <&pgc_mediamix>;
status = "disabled";
lvds-channel@0 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;
phys = <&ldb_phy1>;
phy-names = "ldb_phy";
status = "disabled";
port@0 {
reg = <0>;
ldb_ch0: endpoint {
remote-endpoint = <&lcdif2_disp_ldb_ch0>;
};
};
};
lvds-channel@1 {
#address-cells = <1>;
#size-cells = <0>;
reg = <1>;
phys = <&ldb_phy2>;
phy-names = "ldb_phy";
status = "disabled";
port@0 {
reg = <0>;
ldb_ch1: endpoint {
remote-endpoint = <&lcdif2_disp_ldb_ch1>;
};
};
};
Thank you in advance!
Best Regards!
Hello,
They are the same, but is needed it if you have the plan to use two lvds.
Regards
Hello, thank you for your answer.
Thank you in advance!