LUT - The lookup table (LUT) is used to modify pixels in a manner that is not linear.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LUT - The lookup table (LUT) is used to modify pixels in a manner that is not linear.

2,421 Views
Alex_04
Contributor I

Hi

Asper IMX6SDLRM

53.3.15 LUT  The lookup table (LUT) is used to modify pixels in a manner that is not linear and that

cannot be achieved by the color space conversion modules.  Nonlinear response to the input pixels can be achieved based on how the lookup table is

programmed.

Could you please let me know whether BSP[Linux Kernel] can support the LUT Especially [53.3.15 LUT].

Regards,

Alex

0 Kudos
8 Replies

1,572 Views
Yuri
NXP Employee
NXP Employee

I am afraid Freescale BSP does not support IPU LUT :
“ the common kernel video API is utilized for setting colors, palette registration,
image blitting and memory mapping. The IPU reads the raw pixel data from the
frame buffer memory and sends it to the panel for display.”

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,572 Views
Alex_04
Contributor I

Hi,

Thanks for the information. Searching for LUT(lookup table) in Pixel Pipeline (PXP) in IMX6SDLRM. [chapter : 53.3.15 LUT]

Following the pxp_lib_test in imx-linux-test-imx, for Kernel 3.10.17,

Able to enable in Kernel Configuration

CONFIG_MXC_PXP_V2=y

CONFIG_MXC_PXP_CLIENT_DEVICE=y

CONFIG_DMA_ENGINE=y

Able to find the corresponding node /dev/pxp_device.

Interrupt and its service are registerd in cat /proc/interrupts

130:      0  

GIC  pxp-dmaengine

Kernel thread and its service , known by ps command

89 root    

0 SW   [pxp_dispatch]

While running the Application

./pxp_test.out -I "-o /home/root/abc.txt " ,  getting warning pxp_dispatch_thread: task is timeout

Please help to resolve the issue , if any body come across the issue.

Unable to see CONFIG_IMX_HAVE_PLATFORM_IMX_PXP in Kernel Configuration.

0 Kudos

1,572 Views
Yuri
NXP Employee
NXP Employee

Please look at the following  thread - if Your i.MX6 SDL supports the PXP


https://community.freescale.com/message/506178

Regards,

Yuri.

0 Kudos

1,572 Views
Alex_04
Contributor I

Hi,

     Yes , I have followed the thread https://community.freescale.com/message/506178,

     In u-boot command line , I am unable to read  PXP [Pixel Pipeline] Registers,

    Using md.w 0x20f0000 1  command to read the PXP [Pixel Pipeline] Register , it hangs.

Please help to read and write PXP Registers

Regards,

Alex

0 Kudos

1,572 Views
Yuri
NXP Employee
NXP Employee

What is part number of Your i.MX6 ?

Regards,

Yuri.

0 Kudos

1,572 Views
Alex_04
Contributor I

Hi

PART NUMBER : MCIMX6S5EVM10AC

Please help out to read and write PXP [Pixel Pipeline]Registers at u-boot command level

Regards,

Alex

0 Kudos

1,572 Views
Yuri
NXP Employee
NXP Employee

Alex,

The PXP is clearly stated
in IMX6SDLCEC, which is Datasheet for MCIMX6S5EVM10AC.

But - looks like - it may be disabled on fuse level. Please check OCOTP_CFG2, bit 31.

(Address 0x021B_C430)
  

 

Regards,

Yuri.

0 Kudos

1,572 Views
Yuri
NXP Employee
NXP Employee

Please refer to the following thread regarding PXP testing

It makes sense to wait final results.

Regards,

Yuri.

0 Kudos