Hi
Asper IMX6SDLRM
53.3.15 LUT The lookup table (LUT) is used to modify pixels in a manner that is not linear and that
cannot be achieved by the color space conversion modules. Nonlinear response to the input pixels can be achieved based on how the lookup table is
programmed.
Could you please let me know whether BSP[Linux Kernel] can support the LUT Especially [53.3.15 LUT].
Regards,
Alex
I am afraid Freescale BSP does not support IPU LUT :
“ the common kernel video API is utilized for setting colors, palette registration,
image blitting and memory mapping. The IPU reads the raw pixel data from the
frame buffer memory and sends it to the panel for display.”
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for the information. Searching for LUT(lookup table) in Pixel Pipeline (PXP) in IMX6SDLRM. [chapter : 53.3.15 LUT]
Following the pxp_lib_test in imx-linux-test-imx, for Kernel 3.10.17,
Able to enable in Kernel Configuration
CONFIG_MXC_PXP_V2=y
CONFIG_MXC_PXP_CLIENT_DEVICE=y
CONFIG_DMA_ENGINE=y
Able to find the corresponding node /dev/pxp_device.
Interrupt and its service are registerd in cat /proc/interrupts
130: | 0 | GIC pxp-dmaengine |
Kernel thread and its service , known by ps command
89 root | 0 SW [pxp_dispatch] |
While running the Application
./pxp_test.out -I "-o /home/root/abc.txt " , getting warning pxp_dispatch_thread: task is timeout
Please help to resolve the issue , if any body come across the issue.
Unable to see CONFIG_IMX_HAVE_PLATFORM_IMX_PXP in Kernel Configuration.
Hi,
Yes , I have followed the thread https://community.freescale.com/message/506178,
In u-boot command line , I am unable to read PXP [Pixel Pipeline] Registers,
Using md.w 0x20f0000 1 command to read the PXP [Pixel Pipeline] Register , it hangs.
Please help to read and write PXP Registers
Regards,
Alex
Alex,
The PXP is clearly stated in IMX6SDLCEC, which is Datasheet for MCIMX6S5EVM10AC.
But - looks like - it may be disabled on fuse level. Please check OCOTP_CFG2, bit 31.
(Address 0x021B_C430)
Regards,
Yuri.