I am trying to install LTIB for my I.MX6 SoloLite board. I have installed the dependencies and patched LTIB. I am stuck when booting the kernel. Please help me to solve the problem.
After LTIB is configured, I builded the kernel for iMX6 board. I typed the following command in terminal.
~/Documents/imx6install/ltib$ ./ltib
Then I get this error at the end.
gnueabi/bin/ld: cannot find /lib/ld-linux.so.3
collect2: ld returned 1 exit status
make: *** [busybox_unstripped] Error 1
error: Bad exit status from /home/xuan/Documents/imx6install/ltib/tmp/rpm-tmp.35506 (%build)
RPM build errors:
Bad exit status from /home/xuan/Documents/imx6install/ltib/tmp/rpm-tmp.35506 (%build)
Build time for busybox: 5 seconds
Failed building busybox
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed May 29 23:47:56 2013
Ended: Wed May 29 23:48:01 2013
Elapsed: 5 seconds
These packages failed to build:
busybox
Build Failed
Exiting on error or interrupt
I noticed someone uploaded a similar problem. I tried this solution (listed below) but the error was still there.
Failed solution:
Go into ltib/dist/lfs/base_libs/base_libs.spec and find these lines:
# remove absolute paths from text search files (if they exist)
perl -w -e '
@ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
exit(0) unless @ARGV;
Remove the last two (the lines beginning with "@ARGV" and "exit(0)" and you should be good to go.
Any solutions?
已解决! 转到解答。
Hi, XuanKong,
1) install patch-ltib-ubuntu12.04.sh from (https://community.freescale.com/docs/DOC-93455).
2) create a soft link under /usr/include.
sudo ln -s i386-linux-gun/sys sys
3) install additional packages.
sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev
sudo apt-get install texinfo
4) modify ltib/dist/lfs-5.1/base_libs/base_libs.spec.
...
perl -w -e '
# @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
# exit (0) unless @ARGV;
Good Luck!
Hi, XuanKong,
1) install patch-ltib-ubuntu12.04.sh from (https://community.freescale.com/docs/DOC-93455).
2) create a soft link under /usr/include.
sudo ln -s i386-linux-gun/sys sys
3) install additional packages.
sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev
sudo apt-get install texinfo
4) modify ltib/dist/lfs-5.1/base_libs/base_libs.spec.
...
perl -w -e '
# @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
# exit (0) unless @ARGV;
Good Luck!
I have not re-worked the 12.04 patch :smileysad: so there is no 13.04 yet.
Try 12.04. With latest BSP (4.0.0), there is no need to patch LTIB, but in case you face some issues the first time you run ltib, then apply the patch.
Leo