LTIB building err for imx6q_sabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LTIB building err for imx6q_sabresd

跳至解决方案
4,038 次查看
MarcLiu
Contributor II

Hi, when i building imx6 BSP L3.0.35_4.1.0_130816 in ubuntu 12.04-64bit,get a err: can't compile a simple hello world test program.

liusf@ubuntu:~/imx6/L3.0.35_4.1.0_130816_source/source/ltib$ ./ltib

sh: 2: /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc: not found

Error /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc can't compile a simple hello world test program:

echo '#include <stdio.h>

int main() { printf("hello world"); }' | /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc -x c - -c -o /dev/null

traceback:

main::check_toolchain_setup:2625

  main::pre_build_checks:1465

   main:569

Started: Thu Jun 12 19:27:04 2014

Ended:   Thu Jun 12 19:27:07 2014

Elapsed: 3 seconds

Build Failed

And i found the PATH is including the arm-none-linux-gnueabi-gcc (/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin), but i still get the err, who can help me ?

liusf@ubuntu:~/imx6/L3.0.35_4.1.0_130816_source/source/ltib$ $PATH

bash: /home/liusf/bin:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin:/home/liusf/bin/fsl-linaro-toolchain/bin: No such file or directory

标签 (1)
0 项奖励
1 解答
1,987 次查看
MarcLiu
Contributor II

This problem had solved.

The methods is:

$ sudo aptitude install ia32-libs



在原帖中查看解决方案

0 项奖励
11 回复数
1,987 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi liusf,

I know you are using 64bit ubuntu,  so you please install the following packages :

# Install packages needed by LTIB

sudo aptitude -y install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev

sudo aptitude -y install libdbus-glib-1-dev liborbit2-dev intltool

sudo aptitude -y install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool

sudo aptitude -y install uuid-dev liblzo2-dev

sudo aptitude -y install tcl dpkg

sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev

# Packages required for 64-bit Ubuntu

# Do "uname -a" and see if the word "x86_64" shows up.

if uname -a|grep -sq 'x86_64'; then

sudo aptitude -y install ia32-libs libc6-dev-i386 lib32z1

fi

# The following recommended for Linux development.

# They are not required by LTIB.

sudo aptitude -y install gparted emacs22-nox openssh-server

sudo aptitude -y install nfs-common nfs-kernel-server lintian

sudo aptitude -y install git-core git-doc git-email git-gui gitk

sudo aptitude -y install diffstat indent tofrodos fakeroot doxygen uboot-mkimage

sudo aptitude -y install sendmail mailutils meld atftpd sharutils

sudo aptitude -y install manpages-dev manpages-posix manpages-posix-dev linux-doc

sudo aptitude -y install vnc4server xvnc4viewer

Have a great day,

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,987 次查看
MarcLiu
Contributor II

Hi,Dan

Thanks for your help, the problem has solved .

I have a another problem: when i get android source code , i get a err.

liusf@ubuntu:~/myandroid$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

% Total % Received % Xferd Average Speed Time Time Time Current

Dload Upload Total Spent Left Speed

0 0 0 0 0 0 0 0 ::-- 0:01:04 ::-- 0curl: (7) Failed to connect to 2404:6800:4005:807::100a: Network is unreachable

Has there another url to get repo? or how to solve this problem?

Best Regards

liusf

0 项奖励
1,987 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi liusf,

Which version android source code are you downloading? The problem you attached is the the network server problem, I have met this problem before. After I set proxy server by "export http_proxy=******and export https_proxy=" in my office, it worked. So you also need to set the proxy server first. Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Helpful Answer/ Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,987 次查看
MarcLiu
Contributor II

Hi,Dan

The version is android-4.3_r2.1 that i downloading.

If it is network server problem, the cmd: "$ sudo apt-get install rpm " will fail ,but it succeed, and many other packegs all get succeed.

Best Regards

liusf

0 项奖励
1,987 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi liusf,

You can have a try use : curl "http://php.webtutor.pl/en/wp-content/uploads/2011/09/repo"> ~/bin/repo . Here I attached a file for you . This may help you.

Best Regards
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,987 次查看
MarcLiu
Contributor II

Hi,Dan

I download the android source using : curl "http://php.webtutor.pl/en/wp-content/uploads/2011/09/repo"> ~/bin/repo .

It succeed ,but the following cmd is fail. What can I do?

liusf@ubuntu:~/myandroid$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest-b android-4.3_r2.1

fatal: remote error: Git repository not found

fatal: cannot obtain manifest https://android.googlesource.com/platform/manifest-b

Best Regards

liusf

0 项奖励
1,987 次查看
MarcLiu
Contributor II

Hi,Dan

I have another question about ltib building on 64bit ubuntu. The err info is :

liusf@ubuntu:~/imx6/L3.0.35_4.1.0_130816_source/source/ltib$ ./ltib

Processing platform: Freescale iMX6x Based Boards

===================================================

using config/platform/imx/.config

Processing: fake-provides

===========================

Processing: u-boot-v2009.08

=============================

Processing: kernel-3.0.35

===========================

Processing: skell

===================

Processing: base_libs

=======================

Processing: busybox

=====================

Processing: libtermcap

========================

Processing: bash

==================

Processing: zlib

==================

Processing: iproute

=====================

Processing: hotplug

=====================

Processing: glib2

===================

Processing: alsa-lib

======================

Processing: libxml2

=====================

Processing: udev

==================

Processing: liboil

====================

Processing: gstreamer-core

============================

Processing: gst-plugins-base

==============================

Processing: gst-plugins-good

==============================

Build path taken because: directory build, no prebuilt rpm,

scbuild/scdeploy already unpacked package

Processing: gst-plugins-good

==============================

Build path taken because: directory build, build key set, no prebuilt rpm,

rpmbuild --dbpath /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/tmp' --define '_rpmdir /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec

Building target platforms: arm

Building for target arm

Executing(%build): /bin/sh -e /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/tmp/rpm-tmp.28211

+ umask 022

+ cd /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rpm/BUILD

+ cd gst-plugins-good-0.10.30

+ export CAIRO_CFLAGS=-I/home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rootfs/usr/include/cairo

+ export CAIRO_LIBS=-L/home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rootfs/usr/lib/cairo

+ export LIBS=-lcairo

+ ./configure --prefix=/usr --host=arm-linux --build=x86_64-unknown-linux-gnu --without-check --disable-speex --disable-shout2test --disable-shout2 --disable-dv1394 --disable-libpng --disable-libdv --disable-libcaca --disable-ladspa --disable-jpeg --disable-flac --disable-esd --disable-esdtest --disable-cairo --disable-aalib --disable-aalibtest --disable-x --disable-xvideo --disable-hal NM=nm

configure: WARNING: unrecognized options: --without-check, --disable-ladspa

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for arm-linux-strip... arm-linux-strip

checking for a thread-safe mkdir -p... /bin/mkdir -p

checking for gawk... no

checking for mawk... mawk

checking whether make sets $(MAKE)... yes

checking nano version... 0 (release)

checking whether to enable maintainer-specific portions of Makefiles... no

checking build system type... x86_64-unknown-linux-gnu

checking host system type... arm-unknown-linux-gnu

checking how to print strings... printf

checking for style of include used by make... GNU

checking for arm-linux-gcc... gcc

checking whether the C compiler works... no

configure: error: in `/home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/rpm/BUILD/gst-plugins-good-0.10.30':

configure: error: C compiler cannot create executables

See `config.log' for more details

error: Bad exit status from /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/tmp/rpm-tmp.28211 (%build)

RPM build errors:

Bad exit status from /home/liusf/imx6/L3.0.35_4.1.0_130816_source/source/ltib/tmp/rpm-tmp.28211 (%build)

Build time for gst-plugins-good: 5 seconds

Failed building gst-plugins-good

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Fri Jun 13 01:54:00 2014

Ended: Fri Jun 13 01:54:11 2014

Elapsed: 11 seconds

These packages failed to build:

gst-plugins-good

Build Failed

What I can do for the err?

Best Regards

liusf

0 项奖励
1,987 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi liusf,

If you have any new question/problem, it is better to create another new post. Thanks.:smileyhappy:

Have a great day,

Dan

0 项奖励
1,987 次查看
MarcLiu
Contributor II

Hi, Dan

I get it ,i will create a new post ,thanks for your reply.

Best Regards

liusf

0 项奖励
1,987 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi liusf,

Are you building Multimedia Codecs Source? If yes, please go to edit the ltib/dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec

use # to comment out the followings cairo things like this :

#export CAIRO_CFLAGS=-I/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/include/cairo

#export CAIRO_LIBS=-L/home/ashish/Desktop/dev_imx6/ltib/rootfs/usr/lib/cairo

#export LIBS=-lcairo

Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,988 次查看
MarcLiu
Contributor II

This problem had solved.

The methods is:

$ sudo aptitude install ia32-libs



0 项奖励