LTIB Image file size estimation and NAND Compression techniques.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB Image file size estimation and NAND Compression techniques.

ソリューションへジャンプ
1,031件の閲覧回数
VikramU_ng
Contributor III

Dear Support,

   is there an estimate available on the actual root image file sizes when LTIB is built for a specific architecture. I understand the PDK comes with 2GB NAND. Is there a rough guide on the kernel and the rootfs filesizes in advance?.

net@net-PC:~/Qt_imx257/ltib/rootfs$ ls -lh root*


net@net-PC:~/Qt_imx257/ltib/rootfs$ cd ..
net@net-PC:~/Qt_imx257/ltib$ ls -lh root*
-rw-r--r--  1 net net  15M 2011-09-13 21:56 rootfs.cramfs
lrwxrwxrwx  1 net net   15 2011-09-13 21:56 rootfs_image -> ./rootfs.cramfs

 

Is the current filesize seen for the Image correct?. I have been unable to find resources to compress/compare various image formats. Could someone provide any specific document on this?.

 

 

regards,

Vikram U
タグ(1)
0 件の賞賛
返信
1 解決策
904件の閲覧回数
VikramU_ng
Contributor III

A year later..

   i think the reliable guide is to identify the Base package - 300MB and then add the packages that need to go in.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
905件の閲覧回数
VikramU_ng
Contributor III

A year later..

   i think the reliable guide is to identify the Base package - 300MB and then add the packages that need to go in.

0 件の賞賛
返信