LTIB-ERROR-MPC5125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB-ERROR-MPC5125

495件の閲覧回数
geekdarcy
Contributor III

Hi,

 

I am trying to install LTIB from MPC512xADS_20090603-ltib.ISO for MPC5125 under Ubuntu 12.04 32 bit.

the build fails and I get the following error:

Processing: rpm-fs
====================
ERROR: /tmp/rpm-geekdarcy/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm
would clobber '/reescale/ltib'
traceback:
 main::check_host_clobber:2665
  main::build_rpm:906
   main::f_buildrpms:980
    main::check_rpm_setup:2396
     main::host_checks:1423
      main:542

Started: Mon Nov  5 22:32:49 2018
Ended:   Mon Nov  5 22:32:49 2018
Elapsed: 0 seconds

Build Failed

And I have installed ubuntu-ltib-patch.

This is my first time using LTIB to build a BSP.

Does anyone know what I am doing wrong? Any clue about that error?
 
Kind regards!
タグ(2)
0 件の賞賛
返信
0 返答(返信)