LPPDDR4 Part obsolete || MT53E1536M32D4DT-046 WT:A (Micron)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPPDDR4 Part obsolete || MT53E1536M32D4DT-046 WT:A (Micron)

1,167 Views
JyotiVaishnav
Contributor II

Hello NXP Team, 

The qualified LPDDR part for IMX8M PLUS processor is obsolete.

Can you please share an other 4GB LPDDR part which are compatible with IMX8M PLUS processor.  

Waiting for your reply. 

0 Kudos
Reply
6 Replies

1,127 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

We do not have a list of recommended part numbers.

I suggest you select a LPDDR memory according to the hardware developer's guide and just to be safe on your design I would suggest to re-calibrate and run the DDR stress tool:

i.MX 8M Family DDR Tool Release 

This would help on getting configuration for your new DDR.

Best regards.

0 Kudos
Reply

1,104 Views
JyotiVaishnav
Contributor II

Hello @JorgeCas 

Can we use the MT53E1G32D2FW-046 WT:B LPDDR part with IMX8M PLUS processor. 

0 Kudos
Reply

1,099 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I do not have access to the hole information of selected part number, such as datasheet but, from general information on internet seems it should work ok. I suggest double check with hardware developer's guide.

Best regards.

0 Kudos
Reply

1,084 Views
JyotiVaishnav
Contributor II

Hello @JorgeCas 

Can we use the samsung K4FBE3D4HB-KHCL LPDDR part with IMX8M PLUS processor. 

0 Kudos
Reply

1,064 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello @JyotiVaishnav , apologies for the delay.

I checked the general features about the mentioned part number and also seems ok to be used on your design.

Best regards.

0 Kudos
Reply

1,073 Views
JyotiVaishnav
Contributor II

@JorgeCas 

Awaiting for you reply. 

0 Kudos
Reply