LPDDR2 frequency change in imx6solo ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPDDR2 frequency change in imx6solo ?

574 次查看
ela_embedded
Contributor I

we are using micron LPDDR2  interfaced with imx6solo in our customized board . DDR has three modes of speed grade with 533MHZ , 400 MHZ and 333 MHZ  . we need to configure our mmdc to 333MHz  for power optimization . Is this possible ? i have  gone through the reference manual but i didnt found the required information for mmdc.

标签 (1)
标记 (2)
0 项奖励
1 回复

490 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ela

yes this is possible, for procedure one can look at attached document

Chapter 21 Dynamic Bus Frequency Driver from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励