LPDDR2 and NAND boot for IMX6 Solo.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPDDR2 and NAND boot for IMX6 Solo.

1,499 次查看
sanjayshekar
Contributor I

Hello NXP / Freescale,

             Happy New year and wishing you all the best for the combined venture.

For our new product we are using IMX6 Solo Processor and our hardware engineers have selected the following

RAM : LPDDR2 (MT42L256M32D2LG-18 WT) .

My Questions on this RAM Interface:

1. To Run android, LPDDR2 initialization code changes should be done in only U-Boot code ?? or any Linux code change is needed ??

2. Any Document or patch available for making these changes.

NAND Flash : 1GB MT29F1G08ABBEAH4-AITX:E

1. What is the minimum nand required to run Android latest version (4.4 or 5.0), I see for MMC it says 2GB.

2. How do we flash u-boot code to nand, I have seen people taking about kobs-ng and bootlets,  these tools can be used by running something (u-boot or linux) from SD card or how the NAND is detected as /dev/mtd0?? is it in host machine or on device ??

I know some questions are really basics, but it will be great full if answered..  :smileyhappy:

Regards,

Sanju.

标签 (3)
0 项奖励
回复
5 回复数

1,277 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sanjai

1. modifications should be done in uboot, one can look at attached document

Chapter 1 Porting U-Boot, sect.1.3.1 Changing the DCD Table

2. nand is programmed using MFG Tools with nand on device.

Programmers (Flash, etc.) (9)

IMX-L5.0.0-MFG-TOOL (REV L5.0.0_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,277 次查看
sanjayshekar
Contributor I

Hello Igor,

          Thanks for your reply.. I guess attachment mentioned by you is missing.

Also my question regarding, what is the Minimum NAND flash required for getting all the partition done for Android up running ??

Regards,

Sanju.

0 项奖励
回复

1,277 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sanju

for attachment click on red in previous answer.

1.jpg

~igor

0 项奖励
回复

1,277 次查看
sanjayshekar
Contributor I

Thanks,
I don know why this attachment was not seen yesterday.

Also my question regarding, what is the Minimum size of NAND flash required for getting all the partition done for Android up running including file system??

Hope this time you wont miss this question and close this thread :smileyhappy:

Regards,

Sanju.

0 项奖励
回复

1,277 次查看
igorpadykov
NXP Employee
NXP Employee

as this is common android question suggest

to post it on Developer Support | Android Developers

Best regards

igor

0 项奖励
回复