Hello NXP / Freescale,
Happy New year and wishing you all the best for the combined venture.
For our new product we are using IMX6 Solo Processor and our hardware engineers have selected the following
RAM : LPDDR2 (MT42L256M32D2LG-18 WT) .
My Questions on this RAM Interface:
1. To Run android, LPDDR2 initialization code changes should be done in only U-Boot code ?? or any Linux code change is needed ??
2. Any Document or patch available for making these changes.
NAND Flash : 1GB MT29F1G08ABBEAH4-AITX:E
1. What is the minimum nand required to run Android latest version (4.4 or 5.0), I see for MMC it says 2GB.
2. How do we flash u-boot code to nand, I have seen people taking about kobs-ng and bootlets, these tools can be used by running something (u-boot or linux) from SD card or how the NAND is detected as /dev/mtd0?? is it in host machine or on device ??
I know some questions are really basics, but it will be great full if answered.. :smileyhappy:
Regards,
Sanju.
Hi Sanjai
1. modifications should be done in uboot, one can look at attached document
Chapter 1 Porting U-Boot, sect.1.3.1 Changing the DCD Table
2. nand is programmed using MFG Tools with nand on device.
Programmers (Flash, etc.) (9)
IMX-L5.0.0-MFG-TOOL (REV L5.0.0_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks for your reply.. I guess attachment mentioned by you is missing.
Also my question regarding, what is the Minimum NAND flash required for getting all the partition done for Android up running ??
Regards,
Sanju.
Hi Sanju
for attachment click on red in previous answer.
~igor
Thanks,
I don know why this attachment was not seen yesterday.
Also my question regarding, what is the Minimum size of NAND flash required for getting all the partition done for Android up running including file system??
Hope this time you wont miss this question and close this thread :smileyhappy:
Regards,
Sanju.
as this is common android question suggest
to post it on Developer Support | Android Developers
Best regards
igor