Hi,
I am trying to compile kernel source ( rel_imx_4.1.15_1.1.0_ga) with imx_v6_v7_defconfig for my iMX6Q SABRE AI EVK. But I am getting the following error,
make -j4 uImage LOADADDR=0x10008000
.
.
.
LINK vmlinux
LD vmlinux.o
MODPOST vmlinux.o
GEN .version
CHK include/generated/compile.h
UPD include/generated/compile.h
CC init/version.o
LD init/built-in.o
drivers/built-in.o: In function `mxsfb_probe':
debugfs.c:(.text+0x459dc): undefined reference to `mxc_dispdrv_gethandle'
make: *** [vmlinux] Error 1
Please suggest the correct configuration for SABRE AI board.
My aim is to test hibernation (suspend-to-disk) on the same board with a gstreamer based audio/video Qt5 application, and i found that kernel 4.1.15 have support for the same. Has this been tried before? Is there any known issues with hibernation (supend-to-disk) on ARM?
Thanks and Regards,
Shyam
I have the same error with rel_imx_4.1.15_1.1.0_ga
Is there a patch to solve this?
The defconfig to be used is imx_v7_defconfig instead of imx_v6_v7_defconfig.
Hi Fabio, I have met the same thing Wichi defconfig i.Max6Q use?imx_v6_v7_defconfig can not work . you mean imx_v7_defconfig can support i.Max6Q?
Hi Wen,
Yes, imx_v7_defconfig supports all mx6 SoCs.
Not sure what you mean by i.mx6maxq though.
Thank you Fabio. I use imx_v7_defconfig to make a kernel, it works.
are you following the steps in Yocto User's Guide to build the BSP?
Hi jimmychan,
No, I got the rel_imx_4.1.15_1.1.0_ga kernel source code from freescale git and i am just running the commands
make imx_v6_v7-defconfig
make -j4 uImage LOADADDR=10008000
Note: imx_v7_defconfig seems working fine with imx6q sabre AI board
Thanks
shyam
Maybe I have a solution for you. It seems that the imx_v6_v7-defconfig has some incompatibilities.
At least I finished a compilation with attached .config-file. Would you give it a try?
Unfortunately the Kernel doesn't start completely. It seems to stuck after about 3 to 4 seconds at different states.