I am following i.MX Yocto Project User's Guide from https://www.nxp.com/docs/en/user-guide/i.MX_Yocto_Project_User%27s_Guide_Linux.pdf
I was able to build it and flash it successfully but while booting I am getting kernel crash.
Can anybody please let me know what could be the issue?
I using IMX 7 sabre dual board. I've attached the complete log.
Kernel BUG at 8009fdac [verbose debug info unavailable] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP ARM Modules linked in: CPU: 0 PID: 1 Comm: ���per/0 Not tainted 4.1.44-fslc+g6c1ad�� C r : [<80942160>] psr: a00001d3 0+0x60/0x84)���hU�����[<80942160>] (__do_kernel_fault.part.0) from [<8001f888>] (do_page_fault+0x38c/0x3a0)��`Oł[<8001f888>] (do_page_fault) from [<8001f9dc>] (do_tr� Booting Linux on physical CPU 0x0 Linux version 4.1.44-fslc+g6c1ad49 (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #1 SMP PREEMPT Fri Sep 21 12:24:20 IST 2018 CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX7D SabreSD Board Reserved memory: created CMA memory pool at 0xac000000, size 320 MiB Reserved memory: initialized node linux,cma, compatible id shared-dma-pool Memory policy: Data cache writealloc PERCPU: Embedded 13 pages/cpu @ab71a000 s21068 r8192 d23988 u53248 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Hi sagar
one can try to rebuild image from scratch and use for programming image mfg tool from
Please use mfg tool version corresponding to used linux kernel version.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------