Hello,
I'm trying to run the kernel 3.0.15 on a imx53-based board (it's a NOVPECK). I successfully added the kernel that I catch from freescale's git on LTIB and compile it very well, but, when I try to boot it, I get this log on console:
U-Boot 2009.08-svn226 (Feb 15 2012 - 08:19:29)
CPU: Freescale i.MX53 family 1.0V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 800MHz
mx53 pll3: 216MHz
mx53 pll4: 595MHz
ipg clock : 80000000Hz
ipg per clock : 66666666Hz
uart clock : 21600000Hz
cspi clock : 54000000Hz
ahb clock : 160000000Hz
axi_a clock : 400000000Hz
axi_b clock : 266666666Hz
emi_slow clock: 266666666Hz
ddr clock : 400000000Hz
esdhc1 clock : 160000000Hz
esdhc2 clock : 160000000Hz
esdhc3 clock : 160000000Hz
esdhc4 clock : 160000000Hz
nfc clock : 33333333Hz
Board: NOVPEK i.MX53 1.0 [Boot Reason: [POR]
Boot Device: SD
I2C: ready
DRAM: 512 MB
NAND: No NAND device found!!!
0 MiB
MMC: FSL_ESDHC: 0
In: serial
Out: serial
Err: serial
Hit any key to stop autoboot: 0
MMC read: dev # 0, block # 2048, count 8192 partition # 0 ...
8192 blocks read: OK
## Booting kernel from Legacy Image at 70800000 ...
Image Name: Linux-3.0.15-01244-g34621b4-dirt
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2621556 Bytes = 2.5 MB
Load Address: 70008000
Entry Point: 70008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
�8<�<��8�88���8�8��8��8<�<��8��8�����8���8�<�8�8�<��8��������8�<���8�����������8��8��8�<� �< 8��8�8�8�8���8��8��8�8�
So, after uncompress the kernel, nothing but trash pops up on console. I'm just tired and ran out of ideas. Anybody already had this problem?
My printenv:
NOVPEK_i.MX53_U-Boot> printenv
bootdelay=3
baudrate=115200
ethaddr=88:77:66:55:34:12
ipaddr=192.168.1.201
gatewayip=192.168.1.1
netmask=255.255.255.0
hostname=NOVPEK
loadaddr=0x70800000
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
loadk=mmc read 0 ${loadaddr} 0x800 0x1800
bootcmd_mmc=run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 0x800 0x2000;bootm
bootcmd_nfs=run bootargs_base bootargs_nfs; mmc read 0 ${loadaddr} 0x800 0x2000; bootm
serverip=192.168.15.132
nfsroot=/opt/freescale/rootfs
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp video=mxcdi0fb:RGB565,240x320M-16@15 nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd=run bootcmd_mmc
bootargs_mmc=setenv bootargs ${bootargs} noinitrd console=tty1 root=/dev/mmcblk0p1 ro rootwait ip=none
bootargs_base=setenv bootargs console=ttymxc0,115200 jtag=on
stdin=serial
stdout=serial
stderr=serial
Environment size: 930/131068 bytes
Regards,
Ricardo
解決済! 解決策の投稿を見る。
Hello,
I have encountered the same problem with kernel 2.6.35 and solved it by editing arch/arm/mach-mx5/clock.c :
line 2129
static struct clk uart_main_clk = {
...
.parent = &pll3_sw_clk, // originally &pll2_sw_clk
...
}
I've tried it on Linux 3.0.15, it worked too, now I can enjoy my kernel panic.
Solution found here (patch included) :
https://community.freescale.com/thread/259422
Regards,
Hubert
I suggest you to use either 2.6.35 from Freescale or the Kernel Mainline (kernel.org).
Kernel 3.0.15 from Freescale was made to be used i.MX6 platforms and wasn't tested on i.MX5x.
If you prefer to use Kernel Mainline, check if all drivers you need are currently there.
Rgds
Rogerio
Hello,
I have encountered the same problem with kernel 2.6.35 and solved it by editing arch/arm/mach-mx5/clock.c :
line 2129
static struct clk uart_main_clk = {
...
.parent = &pll3_sw_clk, // originally &pll2_sw_clk
...
}
I've tried it on Linux 3.0.15, it worked too, now I can enjoy my kernel panic.
Solution found here (patch included) :
https://community.freescale.com/thread/259422
Regards,
Hubert
Oh, I see. Indeed, it make sense.
By now, I'm putting my efforts back to kernel 2.6.35, but as soon as I can, I'll follow your idea. Thank you very much for your help!
Regards,
Ricardo.
Hello,ricardo,
if Hubert's answer is OK, please press "Correct answer" Button !
Thanks !
Weidong
I am not sure the kernel param 'jtag=on' affects something on a normal boot so try to remove it.
Leo
Hello Leonardo,
I've tried your tip, stil the same. One thing: this same u-boot env. works perfectly with kernel 2.6.35. Just config issues or implementation bugs?