Hi All,
I am unsure if how to wire Phy to a i.MX8M procc in RGMii mode of operation.
I am using a SOM from Variscite MX8M as the procc module.
The module has its PHY removed, with pins exposed as per the attached schematic.
Attached are the 2 schematic files.
Particularly my concern of the J1.1 on sch > main >> ENET_PHY_REFR_CLK
Does it need to connect somewhere to the PHY ?
Res strappings A>>E on PHY sch?
Any other apparent faults in the wiring?
Has anybody got a linux driver for this device, to share? (yocto)
Any advise and input will be appreciated.
Thank you.
Regards,
Gerhard
Hi Igor,
Thank you very much for the information pointers.
I have the relevant reference now and will proceed from here.
Regards,
Gerhard Laubscher
Cape Town, South Africa
Hi Gerhard
Variscite boards are supported by its vendor and issue may be posted on
Variscite support portal
i.MX8M RGMII signal description can be found in sect.11.5.4 External signal
description i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply and reference -
I do make use of Varsicite's support service incl h/w overview service.
I wanted alternative input, hence questions here -
From the manual reference I deduce - (for RGMII interface)
1. MDIO has MDC as clock reference -
2. RGMII_TXC/RXC is the relevant clocks between PHY & Processor
3. therefor > ENET_PHY_REFR_CLK, on J1.1 is as I have it, is not connected to PHY (refer my sch)
I do hope that I have made the correct deduction on this.
Regards,
Gerhard
Hi Gerhard
examples of rgmi connections can be found in i.MX8M EVK schematic
Best regards
igor