Hi Sir:
I want to use JTAG to communicate with IMX6UL for debug purpose, but now the JTAG can't communicate with IMX6UL.
I find the signals, TMS, TDI, TCK, NTRST and POR_B, from JTAG are correct, but we can't receive the TDO output from IMX6UL.
My question is how do i check status about ”JTAG_SMODE[1:0]” and the register 0x460 of Boot Fusemap ??? Are there have any hardware pin can check it???
The description about JTAG_SMODE at IMX6ULHDG
The description about r 0x460 of Boot Fusemap at IMX6ULRM
Thanks and Regards,
Bryant Chou
Hello,
i.MX 6UL devices by default are in JTAG enabled mode. I do not think
this is root of the issue. Is the i.MX 6UL working? Please verify the scheme,
using the design checklist and chapter "Avoiding board bring-up problems"
in the Hardware Development Guide.
http://cache.nxp.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf
The following may be helpful.
i.MX6UL Hardware design checklist
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------