JTAG Emualtor for I.MX535

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Emualtor for I.MX535

1,231件の閲覧回数
JohnBritto
Contributor I

Hi,

Which Emulator best suite the I.MX535 Processor ?  Any suggestion for low cost model ?

Regards

Antony

ラベル(1)
0 件の賞賛
8 返答(返信)

1,064件の閲覧回数
hippo
NXP TechSupport
NXP TechSupport

Basically any JTAG debugger, supporting ARM Cortex A8, may be used

with i.MX53. Particularly - ARM Real View ICE may be applied.

Please find an overview of 3rd party development tools for ARM here:

< http://www.freescale.com/files/wireless_comm/doc/brochure/BRTOOLENABLECO.pdf >

please also look at recommended devices in “Emulators/Probes” section

<http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...>

1,064件の閲覧回数
JohnBritto
Contributor I

Thanks Hippo

0 件の賞賛

1,064件の閲覧回数
YixingKong
Senior Contributor IV

John

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this

discussion, or create another discussion.
Thanks,
Yixing

0 件の賞賛

1,064件の閲覧回数
YixingKong
Senior Contributor IV

John

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 件の賞賛

1,064件の閲覧回数
JohnBritto
Contributor I

Thanks Weidong

0 件の賞賛

1,064件の閲覧回数
JohnBritto
Contributor I

Weidong,

Say for example if i want to write and execute a stand alone program (LED blink)  (NON-OS & no boot loader) in I.MX535 QSB board i need a IDE and JTAG right? and also if i want to do register level debug ,single step execution for my application code surely i required IDE and JTAG ...please clarify.

Thanks again

Regards

Antony 

0 件の賞賛

1,064件の閲覧回数
Yuri
NXP Employee
NXP Employee

JTAG is needed, as for IDE (Integrated Development Environment) - for simple applications one can use just editor (say, Notepad++), toolchain, and a debugger.  

0 件の賞賛

1,064件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Antony,

    Actually, If your design is based on evaluation board and BSP released by Freescale, Emulator is not required. Normally, emulator can help you do the following jobs:

(1) debug basical system(expecially DDR3 or LPDDR2 etc)

(2)Burn images into flashes on board.

(3)Programing to test performance of your system.

But Freescale provides some necessary tools for those. such as :

MFG Tool for burning ,cfimager for burning, OBDS tool for low level hardware pressing test. etc.

As for settings of memory controller , if the ddr memory you use is different from that of EVK board, you can configure DDR memory controller manually in u-boot (the file's name is flash_header.S)

Regards,

Weidong