Issue about Set the GPIO Voltage on MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue about Set the GPIO Voltage on MX6SL

506 次查看
tony_l_cai
Contributor III

Hi,all

     I use "mxc_iomux_set_specialbits_register(MX6SL_PAD_AUD_MCLK,PAD_CTL_LVE, PAD_CTL_LVE_MASK)", but after I measured,I found the Voltage was not 1.8V, still 3.2v, when the GPIO signal is 1. So could give me some help?

标签 (3)
0 项奖励
回复
1 回复

368 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

please check power-up sequence, otherwise chip may be damaged, as

described in sect.7.2.4 Power-up sequence in low voltage system design

IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite

Just for test one can add 47K pull down to GND on gpio and check if that helps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复