Issue about Set the GPIO Voltage on MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about Set the GPIO Voltage on MX6SL

639 Views
tony_l_cai
Contributor III

Hi,all

     I use "mxc_iomux_set_specialbits_register(MX6SL_PAD_AUD_MCLK,PAD_CTL_LVE, PAD_CTL_LVE_MASK)", but after I measured,I found the Voltage was not 1.8V, still 3.2v, when the GPIO signal is 1. So could give me some help?

Labels (3)
0 Kudos
Reply
1 Reply

501 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

please check power-up sequence, otherwise chip may be damaged, as

described in sect.7.2.4 Power-up sequence in low voltage system design

IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite

Just for test one can add 47K pull down to GND on gpio and check if that helps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply