Issue about Set the GPIO Voltage on MX6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about Set the GPIO Voltage on MX6SL

492件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     I use "mxc_iomux_set_specialbits_register(MX6SL_PAD_AUD_MCLK,PAD_CTL_LVE, PAD_CTL_LVE_MASK)", but after I measured,I found the Voltage was not 1.8V, still 3.2v, when the GPIO signal is 1. So could give me some help?

ラベル(3)
0 件の賞賛
1 返信

354件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

please check power-up sequence, otherwise chip may be damaged, as

described in sect.7.2.4 Power-up sequence in low voltage system design

IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite

Just for test one can add 47K pull down to GND on gpio and check if that helps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛