Is there any way we can configure IMX6Solo at 400Mhz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way we can configure IMX6Solo at 400Mhz

767件の閲覧回数
Yogee
Contributor III

Hi,

We need to understand how IMX6S would be configured at 400Mhz to make the system at lowest power. LPDDR2 used would be configured at 333Mhz.

Yogee

ラベル(1)
タグ(1)
0 件の賞賛
4 返答(返信)

586件の閲覧回数
YixingKong
Senior Contributor IV

Yogee

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛

586件の閲覧回数
YixingKong
Senior Contributor IV

Yogee

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛

586件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

I think you can just use the powersave governor for cpufreq driver, then cpufreq will be fixed at 396MHz.

echo powersave > /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_governor.

0 件の賞賛

586件の閲覧回数
tonyzheng
NXP Employee
NXP Employee

Hi, Yogee

you can refer to i.MX_6Solo6DualLite_Linux_Reference_Manual.pdf.

Maybe you can adopt other methods to realize the objective of low-power consumption. And for example, Low-level Power Management driver on Linux.

As far as i know, IMX6Solo hardware supports four low-power modes: RUN, WAIT, STOP, and DORMANT , you can make the CPU run under these low-power modes.

Regards,

Tony

0 件の賞賛