Is there Android BSP for IMX6 SOLO SABRE SD board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there Android BSP for IMX6 SOLO SABRE SD board?

829件の閲覧回数
sreeharshap
Contributor II

Hello there, 

Is there Android BSP for IMX6 SOLO SABRE SD?

I can see YOCTO is available for IMX6 SOLO SABRE SD but I'm unable to find ANDROID BSP. 

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

651件の閲覧回数
art
NXP Employee
NXP Employee

1. There is no i.MX6Solo SABRE SD board. Only the i.MX6Quad and i.MX6DualLite SABRE SD boards are available from NXP.

2. The current M6.0.1_2.1.0 i.MX6 Android BSP allows to build the target images for all i.MX6 family processors, including the i.MX6Solo. The source code BSP and pre-built demo images for various processors/boards are available here:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/an...

The related documentation is available here:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/an...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

651件の閲覧回数
sreeharshap
Contributor II

Hi Artur

Thanks so much for your prompt update and suggestions.

It was very helpful.

Warm regards

Pole

0 件の賞賛
返信

651件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

one can find android source code and demo image from the link as below:

<Android OS for i.MX Applications Processors|NXP >.

0 件の賞賛
返信