Hi,
according to the website of the SCM-i.MX6 single-chip system module it should be available in industrial temperature grade (-40 to +105°C):
Single Chip Module-i.MX 6D|NXP
However the datasheet section only contains information for the commercial version of the module (0 to 85°C). Is this module now available in industrial grade, or will it be in the future?
Thanks,
Andras
已解决! 转到解答。
Hello,
Preliminary information :
SCM-i.MX 6Dual and SCM-i.MX 6 Quad industrial devices are sampling.
Production in 3Q 2016.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Preliminary information :
SCM-i.MX 6Dual and SCM-i.MX 6 Quad industrial devices are sampling.
Production in 3Q 2016.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------