Is the SCM-i.MX6 available in industrial temperature grade?

cancel
Showing results for 
Search instead for 
Did you mean: 

Is the SCM-i.MX6 available in industrial temperature grade?

Jump to solution
292 Views
andraskormendi
Contributor I

Hi,

according to the website of the SCM-i.MX6 single-chip system module it should be available in industrial temperature grade (-40 to +105°C):

Single Chip Module-i.MX 6D|NXP

However the datasheet section only contains information for the commercial version of the module (0 to 85°C). Is this module now available in industrial grade, or will it be in the future?

Thanks,

Andras

Labels (2)
0 Kudos
1 Solution
126 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

  Preliminary information :
SCM-i.MX 6Dual and SCM-i.MX 6 Quad industrial devices are sampling.

Production in 3Q 2016.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
127 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

  Preliminary information :
SCM-i.MX 6Dual and SCM-i.MX 6 Quad industrial devices are sampling.

Production in 3Q 2016.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos