Hi Asma
seems it is not supported as sect.22.5.9 Receive Control Register (ENETx_RCR)
i.MX6UL Reference Manual describes it: LOOP, in RMII_MODE must be written to 0.
0 Loopback disabled.
https://www.nxp.com/webapp/Download?colCode=IMX6ULRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Asma
seems it is not supported as sect.22.5.9 Receive Control Register (ENETx_RCR)
i.MX6UL Reference Manual describes it: LOOP, in RMII_MODE must be written to 0.
0 Loopback disabled.
https://www.nxp.com/webapp/Download?colCode=IMX6ULRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov, naoumgitnik
https://community.nxp.com/thread/318899.
Can I get the header files for the source code that has been shared on the above link.
#include "enet.h"
#include "eth.h"
#include "macnet.h"/*register definition*/
#include "macnet_hal.h"/*SoC implementation*/
I am working on implementing bare metal program for ethernet MAC RMII mode on MCIMX6G3. looks like the code that you have shared on the above link is relevant to my dev.
Or can I get the freescale driver for MAC on IMX6. I found imx_enet.c on searching google, but I am not sure if its correct?
Regards,
Asma