Hi all,
we are using yocto setup.But we one doubt is it possible to access two machine configurations from single u-boot source bb file ?
machine1 and machine2 configure in sources/meta-fsl-bsp-release/imx/meta-fsl-arm/conf/machine/machine1.conf
like that i gave two machine configurations but i added both machine related patches in u-boot source bb file.
But with out commenting both patch files how can I access one machine patch file in bb file .in bb file
$ vi sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb
From above bb file is it possible to access two different machine configurations by setting machine name
we added the below two lines in above u-boot bb file .
do_patch_prepend(){
if [ "$MACHINE" = "imx6_zcam" ]; then
SRC_URI +="file://0001-imx6_zcam_uboot_customization.patch"
elif [ "$MACHINE" = "imx6_zcam_custom" ]; then
SRC_URI +="file://0002-imx6_zcam_custom_uboot_customization.patch"
else
echo""
fi
}
Then export build directory
$source setenvironment -b build
$vi conf/local.conf
In the above file we gave MACHINE ??=machine1 selected
===========================
Then extract u-boot source
$bitbake u-boot -c unapck -f
====================
Then apply patch
$bitbake u-boot -c patch -f
========================
But patch was not applied .so any body have any idea of that .
$bitbake u-boot -c compile/build -f
i gave its not compiling giving patch was not extract .
Thanks & Regards
veeranjaneyulu
Hi,
try this
do_pre_configure() {
patch -p1 < ${WORKDIR}/<your patchfile name>
}
add the task pre_configure before do_configure, but after after do_patch, also dont give .patch extension to patch file
Hi Pranav Madhu
Thanks for your reply reply.
But i tried no use .its not extracting .I gave normal syntax patch added like SRC_URI+=<"file://patchname">.Its working but i want gave two patch files at the same time for different machine configuration patch files.Is it possible to give ?
Thanks & Regards
veeranjaneyulu
Hi Veeranjaneyulu,
Sorry I'm not sure about it, try to give the do_pre_configure in if-else condition.
Its ok pranav .
Any way thanks for your reply.
Hello Veeranjaneyulu,
It should be theoretically possible to do this, although I haven’t personally tired it. It seems odd that you’re not seeing the patch being applied. Have you tried using MACHINE ??=’machine1‘ on the configuration file and then performing a clean to the recipe to force it to build it from scratch? It may be possible that Bitbake already has the file so does not need to run the tasks again.
Please let us know of your findings!
Regards,
Hello Veeranjaneyulu,
On a second thought, I think the syntax should be like the following to use the value of MACHINE on the logic argument of the function. Perhaps this may help.
if [ "${MACHINE}" = "imx6_zcam" ]; then
SRC_URI +="file://0001-imx6_zcam_uboot_customization.patch"
elif [ "${MACHINE}" = "imx6_zcam_custom" ]; then
SRC_URI +="file://0002-imx6_zcam_custom_uboot_customization.patch"
Thanks for your reply.
I tried like that syntax also but patch was not extracted ,it means in source directory we cant able to get patch related extracted source .Thats we got custom config error issue.
Then compile by using bitbake .Its giving below error .ie reason patch extracting issue.I gave individual buildings .Those builds are compiling and building.
WARNING: /home/vishwa/workspace/checkout_mar16/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb.do_patch is tainted from a forced run
WARNING: /home/vishwa/workspace/checkout_mar16/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb.do_compile is tainted from a forced run
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_compile (log file is located at /home/vishwa/workspace/checkout_mar16/coderepo1/build/tmp/work/imx6_zcam-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.5847)
ERROR: Logfile of failure stored in: /home/vishwa/workspace/checkout_mar16/coderepo1/build/tmp/work/imx6_zcam-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.5847
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc --sysroot=/home/vishwa/workspace/checkout_mar16/coderepo1/build/tmp/sysroots/imx6_zcam imx6_zcam_config
| make: *** No rule to make target `imx6_zcam_config'. Stop.
| make: *** [imx6_zcam_config] Error 1
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/vishwa/workspace/checkout_mar16/coderepo1/build/tmp/work/imx6_zcam-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.5847)
ERROR: Task 4 (/home/vishwa/workspace/checkout_mar16/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 242 tasks of which 240 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/vishwa/workspace/checkout_mar16/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
In U-boot source Make file i customized as per my requirement .ie working but my requirement is how to access from one bb file two different machine patch files .
Hi @veeranjaneyulug did you resolve your issue? I am stuck at the same point. I want to apply same patch for 2 different machines in single .bbappend file