Is i.MX8M Mini Support ATF?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is i.MX8M Mini Support ATF?

Jump to solution
240 Views
Hariharan1
Contributor III

Is that possible to flash Arm Trusted Firmware(ATF) without uboot?

If it is possible, what are the steps i have to follow?

 

Thanks,

0 Kudos
1 Solution
218 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @Hariharan1

Thank you for contacting NXP Support.

Based on the following official documentation from Trusted Firmware, the TF-A binary is combined with U-Boot. Therefore, using the NXP Tools to build the firmware you can't flash only this one.

7.21. NXP i.MX 8M Series — Trusted Firmware-A 2.10.0 documentation

I hope this information will be helpful.

Have a great day!

View solution in original post

0 Kudos
1 Reply
219 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @Hariharan1

Thank you for contacting NXP Support.

Based on the following official documentation from Trusted Firmware, the TF-A binary is combined with U-Boot. Therefore, using the NXP Tools to build the firmware you can't flash only this one.

7.21. NXP i.MX 8M Series — Trusted Firmware-A 2.10.0 documentation

I hope this information will be helpful.

Have a great day!

0 Kudos