Hi,
I would like to try DDR test in the IMX_OBDS for my custom i.MX28 board.
Is the MMU/d-cache enabled during DDR test of OBDS?
OBDS: On-Board Diagnostic Suit for the i.MX28(REV 1)
https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX_OBDS
In addition,
I found following descriptions in the i.MX28 reference manual;
- To accelerate the boot process, the MMU/d-cache is enabled during the time consuming
HAB authentication process (RSA).- MMU and D-Cache are enabled in default to speed up HAB functions
execution speed.
Is the MMU/d-cache enabled during normal boot?
Can someone help me?
已解决! 转到解答。
Hi torus1000
>Is the MMU/d-cache enabled during DDR test of OBDS?
no
>Is the MMU/d-cache enabled during normal boot?
mmu is configured by fuse HW_OCOTP_ROM7:0x8002C210:1 MMU_DISABLE
described in Table 12-9. General ROM Bit in ROM7 OCOTP Bank
i.MX28 Reference Manual
https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus1000
>Is the MMU/d-cache enabled during DDR test of OBDS?
no
>Is the MMU/d-cache enabled during normal boot?
mmu is configured by fuse HW_OCOTP_ROM7:0x8002C210:1 MMU_DISABLE
described in Table 12-9. General ROM Bit in ROM7 OCOTP Bank
i.MX28 Reference Manual
https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------