Hi All,
We want to know the Wi-Fi Direct Support is there or not in Android 7 Released BSP version 7.1.1_1.0.0?
Can we get Wi-Fi Direct Supported BSP Source?
Interfaces:
As per android, Wi-Fi Direct will support with Normal Wi-Fi Mode only.
If we want to enable wifi direct, wifi should be enabled then only we can use wifi direct.
So is there separate interface is created for Wi-Fi[wlan0] & Wi-Fi Direct[p2p0] or It will work with one interface[wlan0] ?
Thanks in Advance!!!!
Regrads,
Raj.