Is OpenCL supposed to work on the iMX6S or iMX6DL? I'm using the latest 4.0.0 release and while clinfo runs (and prints back reasonable numbers) none of the other unit tests run successfully. They all error out with CL_OUT_OF_RESOURCES.
Indeed, it seems like doing just a trivial single line in a kernel such as: output[get_global_id(0)] = 1.0; causes a CL_OUT_OF_RESOURCES error when creating the kernel.
Since Vinvante claims the GC800 series supports GPGPU:
http://www.vivantecorp.com/index.php/en/technology/gpgpu
I thought OpenCL would stand a chance of working on the iMX6S/DL.
Any thoughts?
Solved! Go to Solution.
Hi,
only imx6 quad and dual has OpenCL support.
http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf
regards,
Andre
Hi,
only imx6 quad and dual has OpenCL support.
http://cache.freescale.com/files/32bit/doc/app_note/AN4397.pdf
regards,
Andre