Greetings.
I am working with an iMX35 board (an RPC353) trying to get to work with a 2.6.38 kernel patched for ARM support. The kernel is built and works fine with the board. The remaining issue is enabling the gpio for interrupt handling in our module which previously worked with a .31 kernel.
What I am hoping to find are one or two examples of code for a similar board which use the new functions and interface. In particular
rpc_gpio_input
set_irq_type
request_irq
free_irq
Much obliged,
Jeff Cunningham