Hello All,
Can i.MX6 be interfaced with TI Bluetooth Chip CC256x chip using I2S interface?
If yes, can somebody provide useful documentation/example software for the same.
Thanks in advance!
Best Regards
Hi sameerrapate
yes it can be used with i.MX6 since I2S is industry standard.
I think useful example of I2S connection with i.MX6 can be found on link below
SGTL5000 is supported with i.MX6 for bluetech DEV-i.MX6 V1.1.x board
https://support.bluetechnix.at/releases/imx/mx6/bsp-2.0.0/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Thank you very much for your reply.
What I am looking for is EXTERNAL I2S interface of iMX6 specifically with Bluetooth Chip (ex: TI CC256x chip)
iMx6 (Our Board) <---> TI CC256x chip (External Bluetooth chip).
If you have information regarding the same, please let me know.
I understand SGTL500 is audio codec which is part of iMX6 platform. and interfaced via SSI (I2S).
Thanks a lot!
I am not aware of support this chip on i.MX6 platform.
Best regards
igor
Dear Igor, All,
Thanks for your reply.
Let me put my query in different way.
My set-up would be as follows
1. i.MX6 is a host processor.
2. My intended i.MX6 platform is "RDIMX6SABREAUTO: SABRE for Automotive Infotainment Based on the i.MX 6 Series" which has a BT module connector.
3. External BT chip will be connected to this i.MX6 platforms's "BT module connector" via external interface (Data interface requirement is PCM / I2S)
- I am currently looking for a BT chip which satisfies the above requirement.
- I found that TI bluetooth chip CC256x has PCM / I2S interface.
Considering above set-up, my query is
- Has similar interfacing been done with i.MX6 platform earlier with TI bluetooth chip or any other BT chip?
- If yes, is it possible to provide some documentation/example software for the same?
I hope my query is clear. Let me know if additional details are required..
Best Regards,
Dear Igor, All,
If possible, can I get answer on my above queries?
Best Regards,
Sameer
Hi Sameer
as for me, I am not aware of efforts for support BT with I2S or TI chip on i.MX6 platform.
Some useful links below
https://community.freescale.com/docs/DOC-94235
https://community.freescale.com/docs/DOC-95330
https://community.freescale.com/docs/DOC-95006
Best regards
igor