Hi Michael
it is not recommended to use DMA for BT because depending on the BT service could
be a lot of traffic which the DMA could not handle on time.
There was a similar problems on the i.mx53 solved with attached pacthes, one can try them.
Also it is recommended to try latest BSP, since it fixed many SDMA issues.
L3.10.17_1.0.0_IMX6QDLS_BUNDLE
: Source Code Download Steps Documentation and Demo Images.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
.