Hello,
I am using iMX8QXP processor with linux-imx_5.4.3-1.0.0(linux-imx - i.MX Linux kernel ). I am new to iMX8 series processors and I am trying to interface Quad Flash, Octal Flash, Octal RAM, MCP memory to flexSPI.
I know I can connect Quad/Octal flash to flexspi0 interface, the .dts file is present in source. Change it according to the chip I am using. Create a new driver for the particular chip. Then I can access flash from user space using MTD utils/commands in my application. I have few questions regarding memory access.
1. Is there any example driver which I can go through to create my own flash driver?
2. What is the case if I am using Octal RAM. How can I access it from user space? using MTD utils? Are there any examples?
3. In case of MCP memory(Octal flash + Octal RAM), is it possible to access both Flash and RAM at the same time?
Thank you.
Hi Priyank
1. for driver example one can look at SDK_MEK-MIMX8QX available
on Welcome | MCUXpresso SDK Builder
or linux driver:
spi-nxp-fspi.c\spi\drivers - linux-imx - i.MX Linux kernel
2. unfortunately for Octal RAM I am not aware of any examples, seems MTD utils can be used.
3. I am afraid not.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Since the Octal RAM I am using does not use the SPI NOR commands, I have created kernel driver by taking reference from /driver/mtd/devices/mchp23k256.c from Microchip. I have also changed Kconfig & Makefile accordingly.
I want to connect Octal RAM through flexspi interface. I am confused about the changes I will required to do in my dtsi file.
Right now it contains
&flexspi0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexspi0>;
status = "okay";
flash0: mt35xu512aba@0 {
reg = <0>;
#address-cells = <1>;
#size-cells = <1>;
compatible = "jedec,spi-nor";
spi-max-frequency = <133000000>;
spi-tx-bus-width = <4>;
spi-rx-bus-width = <4>;
};
};
And I want to change it for Octal RAM.
Can you provide some reference for Flexspi RAM(Dual/Quad/Octal) dts file?
I have seen SPI SRAM on the IMX6ul but still not clear how to add for flexspi interface.
Thank you.
Priyank.
Hi Igor
I understand "dts changes are not sufficient and changes in driver are also needed."
I have made necessary changes in driver. I am a little confused about the CS pin.
I am trying to interface Octal RAM in this manner,
where an Octal RAM is in place of Flash A2.
In this case what changes would I need to do in dts file to make the CS pin work?
Will making reg = <1> do this?
Thank you
Priyank
Hi Igor
Thanks for quick reply.
I have already added driver in kernel to support the Octal RAM, made changes in Kconfig and Makefile.
But I am a little confused about the changes in dts file. That is why I need a reference dts file for flexspi RAM(Quad/Octal).
Thank you.
Priyank