Interfacing DDR3 with iMX535

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Interfacing DDR3 with iMX535

跳至解决方案
915 次查看
sherry_zahid
Contributor III

Link me to the documents for interfacing DDR3 with iMX535. Thanks

标签 (1)
1 解答
790 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
791 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

790 次查看
sherry_zahid
Contributor III

Thanks for the response Igor,

Where to obtain IBIS models for the iMX535 DDR3 @ 1.5V and 120 Ohm ODT?

What is the difference between IBIS models with ODT vs Driver impedance?

e.g. what does driver impedance refer to? (these are the names of IBIS models for iMX535)

lpddr2hs_sel10_ds001_mio     -    DDR, 1.2V, lpddr2 mode, 240 Ohm driver impedance

ddr2odths_t21_sel00_mi          -     DDR, 1.8V, ddr2 mode, 21 Ohm ODT

Regards,

0 项奖励
回复