Interfacing DDR3 with iMX535

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing DDR3 with iMX535

ソリューションへジャンプ
916件の閲覧回数
sherry_zahid
Contributor III

Link me to the documents for interfacing DDR3 with iMX535. Thanks

ラベル(1)
1 解決策
791件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
792件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

please check i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

791件の閲覧回数
sherry_zahid
Contributor III

Thanks for the response Igor,

Where to obtain IBIS models for the iMX535 DDR3 @ 1.5V and 120 Ohm ODT?

What is the difference between IBIS models with ODT vs Driver impedance?

e.g. what does driver impedance refer to? (these are the names of IBIS models for iMX535)

lpddr2hs_sel10_ds001_mio     -    DDR, 1.2V, lpddr2 mode, 240 Ohm driver impedance

ddr2odths_t21_sel00_mi          -     DDR, 1.8V, ddr2 mode, 21 Ohm ODT

Regards,

0 件の賞賛
返信