Hello,
I need to play .wav file in IMX8ULP EVK9 from A core, for that i'm using pre built Linux release image which is i downloded from IMX 8ULP EVK.
I'm uisng Linux 6.6.3_1.0.0 pre built image and after apply "aplay -l" command i'm able to see WM8960 sound card.
Now for my project i'm using Linux 6.1.36_2.1.0 release version and i build image using "bitbake imx-image-core" command . In this image when i apply aplay -l command i'm getting following msg.
root@imx8ulp-9x9-lpddr4-evk:~# aplay -l
aplay: device_list:274: no soundcards found...
From menuconfig i have enabled WM8960 support and i'm able to apply modprobe snd_soc_wm8960 command in my image but not able to find soundcard after applying aplay -l command.
So is there any other changes i need to do befor build image?
Thanks
Hello,
Are you using EVK board?
Please also check the device file you have loaded for kernel in the u-boot.