Hi,
I have just acquired the latest imx6 board and i am trying install some libraries in it.
I tried using apt,apt-get commands but that doesnt work as i am using the image given in the box itself.
So can someone please let me know if i can install libraries in the board and if it is possible how to do it?
I am using the board for this 1st time so any help will be really good.
i am using imx6ull and the OS the image has is NXP i.mx Release Distro version 4.9.88-2.0.0
Thanks and Regards,
Athul
hi @Chavira ,
i have build an image using the steps in the guide for IMx6. i can see the file with extension .wic.zst. i would like to know how to flash this into an sdcard.
i understand this is the command to run :
uuu -b sd_all <bootloader> <rootfs (.wic)>
but my problem is i cant understand which bootloader file to use as there as multiple files iwt name u-boot and in this example i can see the files used are having extension sd.bin_flas_evk but i cant find a file with this extension in my folder.
Can you please let me know the file to be used as bootloader.
Also when i try the above command with the file as u-boot.imx i get
Wait for unknown drivers...
kind of errors. even though the card reader is detected by the system.
I am using a VM for building
Please help me if you have any suggestion or solution to this
Hi,
Since i cant install any library i am trying to cross compile the libraries i need to do install using a toolchain the toolchain i am using for the same is https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x...
i am able to compile the boost lib but not the the openssl and vsomeip libs i get compiler broken for vsomeip and crypto/aes/aesv8-armx.S: Assembler messages:
crypto/aes/aesv8-armx.S:4: Error: unknown architecture `armv8-a+crypto' error for openssl
Am i using the wrong toolchain or this is some other issue?
Thanks,
Athul
Hi @athul_am!
You have to compile the toolchain.
Please check the next guide for the same.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Detailed-Operations-For-Standalone-On-Li...
Best Regards!
Chavira
Hi @athul_am!
Thank you for contacting NXP Support!
To add any package based on our BSP you have to compile the image.
You have to add the next on the conf/local.conf .
Examples:
IMAGE_INSTALL += "pcsc-lite"
IMAGE_INSTALL += "pcsc-lite-dev"
IMAGE_INSTALL += "pcsc-lite-lib"
And then compile the image using the command bitbake <image>
The image could be "imx-image-multimedia",
"imx-image-full",
"imx-image-core", etc.
Best Regads!
Chavira