Dear Sir,
Our customer would like camera device and format is 16-bit YCrcb on i.MX51 platform.
We checked the i.MX51 could support it (page1184 on MCIMX51RM.pdf).
We see CSI interface are CS1_D8~D19 *(12-bit) and CS2_D12~D19 (8-bit) (page109~ 113 on MCIMX51RM.pdf).
We don't know how to connect 16-bit at one CSI port.
Could you help confirm it?
Thanks a lot,
解決済! 解決策の投稿を見る。
Hi Andy
for such connections one can look at i.MX53 IPU (its IPU is similar to i.MX51)
datasheet IMX53CEC Table 59. Camera Input Signal Cross Reference, Format and Bits Per Cycle
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Andy
for such connections one can look at i.MX53 IPU (its IPU is similar to i.MX51)
datasheet IMX53CEC Table 59. Camera Input Signal Cross Reference, Format and Bits Per Cycle
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Sir,
Thanks a lot and we will follow IMX53CEC table 59 to connect and test it.