Hi,
I generated initramfs(core-image-minimal-initramfs-imx6ulevk-xxxxx.rootfs.cpio.gz) using core image recipe such as core-image-minimal-initramfs.bb .
From the recipe, package depends on initramfs-live-boot, initramfs-live-install, initramfs-live-install-efi, so what is the major difference between boot, install & efi script. Did i need all the three?
Also, while booting initramfs, i'm getting the following error,
Freeing unused kernel memory: 412K (80a45000 - 80aac000)
mount: mounting /run/media///rootfs.img on /rootfs/ failed: No such file or directory
/init: line 196: can't create : nonexistent directory
/init: line 196: can't create : nonexistent directory
sh: can't access tty; job control turned off
/ #
/ #
Kindly share your thoughts.
Hi Michael
one can look at
regarding dependencies may be recommended to post
on yocto project mail list as this is generic yocto question
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------