Information about temperature calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Information about temperature calibration

ソリューションへジャンプ
1,643件の閲覧回数
sebastiansuesen
Contributor II

Hello,

I want to calibrate the thermal sensor for the imx8mm. I read the i.MX 8M Mini Applications Processor
Reference Manual chapter 5.4 Thermal Monitoring Unit (TMU).

I can't find information about the calibration register for the TE1/TE2 value. All the information I found in the chapter are 8-bit data stored in OTP cells. How is the name of the register?

Do you have an application note, which described the temperature calibration on production test?

I ask because we have our own customer board and want to calibrate the thermal sensor.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,514件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, It came calibrated, but Thermal driver is a necessary driver for monitoring and protecting the SoC. The thermal
driver will monitor the SoC temperature in a certain frequency.

Regards

元の投稿で解決策を見る

3 返答(返信)
1,514件の閲覧回数
sebastiansuesen
Contributor II

Do you know, if I have to calibrate the thermal sensor?

I ask because we get only an imx8mm SOC not a board with the SOC. Do I have to calibrate the SOC or is the SOC calibrated?

0 件の賞賛
返信
1,515件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, It came calibrated, but Thermal driver is a necessary driver for monitoring and protecting the SoC. The thermal
driver will monitor the SoC temperature in a certain frequency.

Regards

1,514件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sebastian,

Seems details can be found only in sources of thermal drivers described in

sect.2.9.3 Source Code Structure of the  Linux reference Manual of the BSP.

Regards

0 件の賞賛
返信