Imx8mm vpu libimxdmabuffer compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx8mm vpu libimxdmabuffer compile error

ソリューションへジャンプ
2,521件の閲覧回数
hello122344
Contributor II

Hi, I'm working with  iMX8mm   i want to use  vpu H264

https://github.com/Freescale/libimxdmabuffer

When following the specified configuration instructions;

./waf configure --prefix=PREFIX

Errors relating to not having a specified kernel headers path appear. So I added the following kernel headers path in the configuration;

./waf configure --prefix=PREFIX --imx-linux-headers-path=/home/jensen/imx8mm/OK8MM-linux-sdk/OK8MM-linux-kernel/include/  

but  Errors  Could not find linux/mxcfb.h in path "/home/jensen/imx8mm/OK8MM-linux-sdk/OK8MM-linux-kernel/include/" specified by --imx-linux-headers-path   But there is linux/mxcfb.h  in this directory

Any suggestions on what could be causing this issue?

Thank you,

jensen

 

 

0 件の賞賛
返信
1 解決策
2,468件の閲覧回数
hello122344
Contributor II

Thank you for your reply..I try the patch。

Best wishes

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
2,516件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

why do you need to install this if you just want to use vpu encoder? the bsp support vpu encoder already as default, you don't need to install this, this isn't official released version, I'm not sure if this is tested on imx8mm board

 

0 件の賞賛
返信
2,510件の閲覧回数
hello122344
Contributor II

hi ,joanxie

Thank you for your reply.

I want to decode USB camera(H264) with vpu,I found libimxvpuapi      https://github.com/Freescale/libimxvpuapi

But libimxdmabuffer is required when compiling

Checking if this combination works : yes
Checking for program 'pkg-config' : /opt/fsl-imx-xwayland/4.14-sumo/sysroots/x86_64-pokysdk-linux/usr/bin/pkg-config
Checking for 'libimxdmabuffer >= 0.9.0' : not found
The configuration failed

Do you have vpu api for imx8mm? Or how to use vpu of imx8mm(usb camera)

think you very much..

Best wishes

0 件の賞賛
返信
2,505件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you tell me what bsp version you use?

 

0 件の賞賛
返信
2,502件の閲覧回数
hello122344
Contributor II

hi joanxie:

     I am using  L4.14.78_1.0.0_ga_MX8MMEVK(LINUX)

 think you

0 件の賞賛
返信
2,475件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I have mailed to you, pls check your mailbox

 

0 件の賞賛
返信
1,588件の閲覧回数
ankitpatel_atp
NXP Pro Support
NXP Pro Support

Hi @joanxie 

Can you share this patch to me ?

I need it for one of the customer.

 

-Ankit.

0 件の賞賛
返信
2,448件の閲覧回数
Bob256
Contributor I

Where is the link to the patch?  Thanks.

0 件の賞賛
返信
2,469件の閲覧回数
hello122344
Contributor II

Thank you for your reply..I try the patch。

Best wishes

0 件の賞賛
返信