iMX8M plus : Androind 11 userdata partition is reformated always after SD card is flashed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M plus : Androind 11 userdata partition is reformated always after SD card is flashed

1,443 Views
swapnilpendhare
Contributor III
It seems the userdata is not accepted by the Android OS and it's formatted on first boot with SD card. I could see some security and partition signature related errors in bootloader, but could not find the root cause. 
 
have attached the Boot log file.
  • If you check like 55 to 65 of the boot log; You will see some issue in the bootloader with partition table magic numbers and it tries to reset metadata. 
Hit any key to stop autoboot:  0
In boota get fastboot lock status error. Set lock status
Magic is incorrect.
Error validating A/B metadata from disk. Resetting and writing new A/B metadata to disk.
Writing A/B metadata to disk.
 verify OK, boot 'boot_a'
Kernel load addr 0x40480000 size 52437 KiB
kernel   @ 40480000 (55246848)
ramdisk  @ 44680000 (12502925)
fdt      @ 43ab0400 (62921)
Moving Image from 0x40480000 to 0x40600000, end=43ab0000
  • Also when the kernel is booted, if you check the logs between line 2069 and 2228 the userdata partition is formatted as it was considered corrupted earlier. 
    [   64.723192][  T229] EXT4-fs (dm-9): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
    [   64.723192][  T229] EXT4-fs (dm-9): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
    [   64.746778][  T229] JBD2: no valid journal superblock found
    [   64.746778][  T229] JBD2: no valid journal superblock found
    [   64.758304][  T229] EXT4-fs (dm-9): error loading journal
    [   64.758304][  T229] EXT4-fs (dm-9): error loading journal
    [   64.773262][  T179] init: Unable to set property 'ro.boottime.init.mount.data' from uid:0 gid:0 pid:229: Read-only property was already set
    [   64.773262][  T179] init: Unable to set property 'ro.boottime.init.mount.data' from uid:0 gid:0 pid:229: Read-only property was already set
    [   64.828382][  T229] e2fsck: WARNING: linker: Warning: "[vdso]" unused DT entry: unknown processor-specific (type 0x70000001 arg 0x0) (ignoring)
    [   64.828382][  T229] e2fsck: WARNING: linker: Warning: "[vdso]" unused DT entry: unknown processor-specific (type 0x70000001 arg 0x0) (ignoring)
    [   64.857711][  T229] e2fsck: e2fsck 1.45.4 (23-Sep-2019)
    [   64.857711][  T229] e2fsck: e2fsck 1.45.4 (23-Sep-2019)
    [   64.874894][  T229] e2fsck: Superblock has an invalid journal (inode 8).
    [   64.874894][  T229] e2fsck: Superblock has an invalid journal (inode 8).
    [   64.888429][  T229] e2fsck: Clear? yes
    [   64.888429][  T229] e2fsck: Clear? yes
    [   64.896057][  T229] e2fsck:
    [   64.896057][  T229] e2fsck:
    [   64.901915][  T229] e2fsck: *** journal has been deleted ***
    [   64.901915][  T229] e2fsck: *** journal has been deleted ***

 

We are currently using ./imx-sdcard-partition.sh provided in imx android build along with all the android images when I build android. Also sharing SD card creating log. 
 
0 Kudos
Reply
0 Replies