Kernel Logs
===============
2.581677] mmc3: new DDR MMC card at address 0001
[ 2.586978] Segment Routing with IPv6
[ 2.590725] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.597817] NET: Registered protocol family 17
[ 2.602326] lib80211: common routines for IEEE802.11 drivers
[ 2.608380] mmcblk3: mmc3:0001 S0J57X 29.6 GiB
[ 2.613214] mmcblk3boot0: mmc3:0001 S0J57X partition 1 31.5 MiB
[ 2.619314] Key type dns_resolver registered
[ 2.624051] mmcblk3boot1: mmc3:0001 S0J57X partition 2 31.5 MiB
[ 2.630269] mmcblk3rpmb: mmc3:0001 S0J57X partition 3 4.00 MiB, chardev (245:0)
[ 2.645896] Registering SWP/SWPB emulation handler
[ 2.651099] Loading compiled-in X.509 certificates
[ 2.658458] mmcblk3: p1 p2
[ 2.683162] A9-M4 sema4 num 6, A9-M4 magic number 0x12345678 - 0xe42be0bd.
[ 2.690765] vddarm: supplied by SW1AB
[ 2.694724] vdd1p1: supplied by VGEN6
[ 2.698604] vdd2p5: supplied by VGEN6
[ 2.702541] vddsoc: supplied by SW1AB
[ 2.709683] imx_thermal tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
[ 2.720389] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 2.738780] EXT4-fs (mmcblk3p2): mounting ext3 file system using the ext4 subsystem
Kernel support enabled for
===
1) ext2
2)ext3
3) ext4
Filesystem partition is ext3 using mfgtool - windows utility
Query
===========
1) What can be reason here to stuck ?
Hi rakesh_patel
EXT4-fs (mmcblk3p2): mounting ext3 file system using the ext4 subsystem
is described for example on
If one uses mfg tool one can try to change mkfs.ext3 in ucl2.xml to mkfs.ext4
or follow i.MX Linux User’s Guide for creating partition.
Best regards
igor
Hi rakesh_patel
one can try to use latest kernels with uuu
Best regards
igor
I have fixed this issue as some kernel configurations and voltage regulator causes the issue in the custom board.
But, I have one query for NXP:
1) mfgtool do ucl2.xml file do ext3 partitions. Is there any reason to choose ext3 as default? Why not ext4?