Imx6sx chip part change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6sx chip part change

425件の閲覧回数
naveenprasath_0
Contributor I

Hi,

Currently, we are using the following imx6sx part in our design :

MCIMX6X4CVM08AC

Is there any software changes required to replace the above part with

MCIMX6X4EVM10AC

The difference between both is the existing part operating frequency is 800MHZ whereas the new part is 1000MHz.

 

Please suggest if it will work without any SW changes?

ラベル(1)
0 件の賞賛
1 返信

419件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Naveen

 

for changes of operating frequency one can consider cpu "operating-points" entries in imx6sx.dtsi :

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx.dtsi?h=imx_5.4.70...

Also for new part recommended to run ddr test

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/11082...

and update uboot dcd header with new ddr settings found from ddr test

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6sxsabresd/imximage.cfg?...

 

Best regards
igor

0 件の賞賛