Imx6 SSI 24Mhz Bit clock generation and 48Khz frame sync clock from pll4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 SSI 24Mhz Bit clock generation and 48Khz frame sync clock from pll4

681 Views
dp_yanam
Contributor I

we are trying to generate 24Mhz bit clock from SSI 48KHz frame sync clock. When i go through the CCM module & other similar questions in NXP.  mentioned like reprogramming the PLL4 to achieve the bit clock 24Mhz.

Please let me know which part of the code in the kernel reprogram the pll4 in the kernel 4.14.

0 Kudos
Reply
2 Replies

644 Views
dp_yanam
Contributor I

Hi igor,

Thanks for your support & information. i could able to achieve the clock frequency by setting post dividers in the clk_imx6q.c

Best regards,
K. durgaprasad

 

0 Kudos
Reply

673 Views
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

 

simple examples for this case can be found in SDK

https://github.com/RT-Thread/rt-thread/tree/master/bsp/imx6sx/iMX6_Platform_SDK

 

>Please let me know which part of the code in the kernel reprogram the pll4 in the kernel 4.14

 

in linux one can look at clk driver:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/clk/imx/clk-imx6q.c?h=imx_4.14.98_...

Documentation

 

Best regards
igor

0 Kudos
Reply