I downloaded the image of the WEC7 from adeneo link and tried to boot the QSB START-R board by following the steps given in “FREESCALE_iMX53_QSB_WEC7_user_guide_V131.pdf”.
I have tried to boot the Start-R board by image "........\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel" by using uSD card by using following commands
cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53
cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\nk.nb0 -d H -imx53 “
After this command if i insert uSD card in START-R board by connecting the power cable and VGA cable, nothing is visible on VGA.
Hi Yuri,
I am using .....\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53 -a command to write on uSD.
and i am getting following message
removable = no
device block size = 512 bytes
device block count = 0x3ad4f0
firmware size = 0x80000 bytes (0x400 blocks)
extra blocks = 1022
Flashing eboot.nb0 at sector 0x2
Writing firmware...
Writing FAT partition...
Writing MBR...
done!
but after making the setup but eboot output not appears on UART.I ma using baud rate as mentioned in doc(115200) and using serial to usb com.